The Alarms API is a service that will generate alerts for configured abnormal conditions. The platform will generate alarms itself, and ingest alarms from other subsystems. Automatically generating an alert allows operators to understand the current condition of the control system, knowing that issues will be brought to their attention automatically.
A single alarm is a state machine, where the transitions are recorded in a log. The state machine is discussed in detail in the document.
The Alarms API consists of two endpoints, alarms and events.
- Events : The events endpoint is a transaction log of all the transitions in the system
- Alarms : The alarms contains a list of all currently unresolved alarms in the platform
The most common usecase is to synchronise with the alarm system, which has two methods available depending on your requirements.
Synchronise every alarm transition.
- Set
lastUpdate
to 0 - Query
/events?lastUpdate={lastUpdate}
- Process all the alarms
- Save the
lastUpdate
value - Go to 2
Get the current alarms and watch future events.
- Query
/alarms
- Process all the alarms
- Save the
lastUpdate
value - Query
/events?lastUpdate={lastUpdate}
- Process the alarms
- Save the
lastUpdate
value - Go to 4
Querying the alarms
or events
end point will return alarm events. The details of each property is discussed below
EventID
Unique identifier for each alarm transition. Primarily used to identify which alarms are being acknowledged, and for the alarm system to forward acknowledgements to the subsystems. Alarm events (EventID) are acknowledged, not alarms (SourceID) themselves. This to avoid race conditions where an alarm that has recently transitioned can be interacted with before the even is displayed to the operator. EventID is always prefixed by the subsystem.
SourceID
Unique identifier of the individual alarm state. An alarm can be in only one state at a time.
If the system is unmanaged, and an incoming alarm events with new EventIDs will replace the alarm that has the same SourceID
.
If the system is managed, and an incoming alarm event with new States will replace the alarm that has the same SourceID
.
SourceID
is always prefixed by the subsystem.
ValueID
Unique identifier of the monitored cocntrol point. Primarily used to gather additional metadata. ValueID is always prefixed by the subsystem.
State
The state is the condition of the alarm The alarm can be in four different states:
State | Description |
---|---|
0 (Invalid) |
Invalid state, transition is ignored |
1 (Active) |
The monitored status is currently in an abnormal condition |
2 (Acknowledged) |
The alarm has been acknowledged |
3 (Reset) |
The monitored status has returned to normal, but has not been acknowledged |
4 (Normal) |
The monitored status has returned to normal, and is not waiting to be acknowledged |
Alarm Lifecycle
Alarms are configured to have a certain lifecycle. Depending on the configuration, the Acknowledged
and Reset
states
may be disabled so that operator interaction is not required to clear the alarms.
Lifecycle | Code | Description |
---|---|---|
Unmanaged |
0 |
The subsystem is responsible for managing the alarm status. Acknowledging an alarm will be forwarded to the subsystem |
ManagedAck |
1 |
The platform will allow operators to acknowledge an alarm, even if the subsystem does not support it |
ManagedRst |
2 |
The platofrm will not allow operators to acknowledge an active alarm, and require an acknowledgement to clear the alarm from the system |
ManagedAckRst |
3 |
The platform will allow operators to acknowledge an active alarm, and require an acknowledgement to clear the alarm from the system |
CanAcknowledge
Can acknowledge indicates whether the alarm can be acknowledged by the operator. The value depends on the alarm lifecycle.
CanAcknowledge | (State) Alarm Lifecycle | Description |
---|---|---|
false |
(any) Unmanaged |
No operation |
true |
(any) Unmanaged |
Alarm acknowledgement is forwarded to the subsystem. The alarm state transition to acknowledged or normal must be sent from the subsystem |
true |
(active) ManagedAck or ManagedAckRst |
Alarm acknowledged event is generated in the platform |
true |
(reset) ManagedRst or ManagedAckRst |
Alarm normal event is generated in the platform |
CanResolve
The alarms from subsystem can get stuck in certain conditions. For example, if an alarm has been activated, then the subsystem is decomissioned - a reset alarm event may never be generated. In this scenario, an operator must manually resolve the alarm state. Typically this is reserved for operators with high level of permissions.