Overview

This API has been designed for Schneider Electric’s (SE) internal use to handle multiple utility providers that are relevant to EcoStruxure products.

At present, the API provides access to electricity consumption data from Enedis Linky meters. The aim is to provide other utility provider data like gas, for as many countries as possible.

To request the addition of more data sources, contact ecostruxure.openness@se.com.

API overview and usage

The API currently supports following.

Utility Type Provider Country Features
Electricity Enedis France
  • Get consent* from Enedis users for access to their Linky meter data.
  • List the meters available from energy provider.
  • Get the daily energy consumption data for a given meter.